Salt River Project Completes Hydropower Modernization Project for Greater Renewable Energy Production Efficiency and Reliability

Fallback image

SRP’s Roosevelt Dam, situated along the Salt River in Arizona, is one of three critical hydropower sites modernized with the Ovation™ Automation Platform to help ensure operational continuity and drive increased performance. Photo credit: SRP. High resolution image

Fallback image

SRP has standardized on Emerson’s Ovation™ Automation Platform for its hydropower fleet, modernizing plant and excitation controls—even at the nearly 120-year-old Roosevelt Dam—to help ensure a reliable, clean, and continuous supply of power for its customers. Photo credit: SRP. High resolution image

Standardizing on Emerson’s Ovation platform, Arizona power provider reduces maintenance costs by 30%, cuts troubleshooting time in half

PITTSBURGH (Sept. 30, 2025) – Emerson, an industrial technology leader delivering advanced automation solutions, today announced the completion of a multi-year modernization project at four Salt River Project (SRP) hydroelectric dams along the Salt River in Arizona. SRP’s Roosevelt, Horse Mesa, Mormon Flat and Stewart Mountain dams generate 265 megawatts of hydropower – enough to power more than 60,000 homes annually. 

SRP modernized its legacy excitation systems – vital for power generation – and seamlessly integrated them with the distributed control systems already in place at its four hydroelectric dams. By standardizing on Emerson’s Ovation™ Automation Platform and implementing modern control strategies, SRP reduced operations and maintenance costs by 30% and cut troubleshooting time by half – helping ensure operational continuity and strengthening grid performance. Enhanced operational visibility keeps critical startup and shutdown procedures efficient, avoiding delays that could have doubled their duration.  

“As the long-time operator of the Bureau of Reclamation’s dams, we have a responsibility to ensure delivery of a reliable, clean and continuous source of power the community depends on,” said Shari Brady, SRP Hydro electrical engineer. “By standardizing on Emerson’s fully unified Ovation automation platform across our hydro fleet for excitation and plant control – and through close collaboration between project teams – we completed all system installations on time, even with aggressive schedules. We now have greater operational insight and easier troubleshooting, which helps us maintain unit reliability in the 90th percentile.”  

Rising electricity consumption driven by record growth in the Phoenix area along with extreme temperatures in the service area have required energy providers like SRP to continue to invest in improving its infrastructure, including generator excitation.   

“Increased visibility and reliability of hydro operations helps Salt River Project ensure continuous operation to efficiently supply their customers with the power they rely on 24/7,” said Bob Yeager, president of Emerson’s power and water business. “SRP’s vision for standardizing on a fully unified automation system was a transformative step that will position them for success –even in the face of shifting energy markets and increased need for power – for decades to come.” 

The custom Ovation™ Excitation Systems,  two of which are for pump and energy storage units that require unique integration when switching to pump mode, are seamlessly integrated into the existing Ovation distributed controls. The new cohesive plant system improves SRP’s hydroelectric capabilities, which help strengthen grid reliability and meet the demands of an evolving grid using more renewable energy resources like solar and wind.  

SRP’s new, fully integrated automation platform simplifies operations and maintenance by using the same spare parts, streamlining training, maintaining operator familiarity and managing a single point of contact for automation support and service. 

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Visit Emerson’s Ovation Automation Platform Page on LinkedIn 
• Connect with Emerson via X Facebook LinkedIn YouTube

About Emerson
Emerson (NYSE: EMR) is a global industrial technology leader that provides advanced automation. With an unmatched portfolio of intelligent devices, control systems and industrial software, Emerson delivers solutions that automate and optimize business performance. Headquartered in St. Louis, Missouri, Emerson combines innovative technology with proven operational excellence to power the future of automation. For more information, visit Emerson.com.