Refine Smarter: Automation Technologies for Lithium Processing Excellence

Lithium Refining

Automation technologies that drive efficient, consistent, and optimized lithium refining for EV battery applications.

Measurement Instrumentation for Optimal Flocculant Management
Discover Solutions

Optimizing Lithium Refining with Advanced Automation and Intelligent Process Control

Increase purity, yield, and sustainability with smart automation across your refining operations

Emerson enables lithium refiners to achieve higher purity, increased yield, and sustainable operations through advanced automation, precise measurement, and intelligent analytics.

Innovative Technologies

EVB Solutions in Action

Emerson’s solutions harness automation technology, software, and services to help industries achieve greater efficiency, enhanced safety, and sustainable operations across the value chain.

Reduce Downtime with Real-Time Monitoring

Reduce Energy Usage and meet Emissions Regulations

Expert Answers for a Rapidly Evolving Industry

Frequently Asked Questions (FAQs)

As global demand for battery-grade lithium accelerates, refining operations face growing pressure to scale efficiently, reduce environmental impact, and ensure product quality. This FAQ section addresses common questions.

Lithium is isolated and refined through a series of chemical processes that transform raw lithium into a saleable form. The process begins with the extraction of lithium-rich minerals from the earth, which can be from hard rock mining or brine extraction. The raw materials are then concentrated to separate lithium from other minerals, using techniques like crushing and grinding, flotation, and leaching. The refined lithium is then purified through precipitation and filtration to achieve high purity levels, making it suitable for use in batteries and other applications.

Critical raw materials used in manufacturing Li-ion batteries (LIBs) include lithium, graphite, cobalt, and manganese. As electric vehicle deployments increase, Lithium EV battery production for vehicles is becoming an increasingly important source of demand.

Lithium battery component (or battery cell) manufacturing is done in sets of electrodes and then assembled into battery cells. To produce electricity, lithium EV batteries shuttle lithium ions internally from one layer, called the anode, to another, the cathode. The two are separated by yet another layer, the electrolyte.

Every generation of battery design – cylindrical, prismatic, polymer pouch, and now, solid state - challenges technical limits and demands more from battery assembly technology. Ultrasonic welding solutions reliably bond the thinner, more delicate metals and advanced hybrid films needed to build more energy-dense batteries.

 

The extraction of lithium is currently restricted to Australia, Chile, and Argentina and to a few companies, with only four businesses controlling almost 60% of global production. However, the boom in lithium over recent years has demonstrated that the lithium market is facing major changes. Alongside the expansion of existing facilities, large-scale projects are being planned and implemented in other countries, such as Canada, Mexico, and Bolivia. Europe also has significant potential.