Emerson’s Upgraded Handheld Device Communicator Helps Personnel Deliver Faster, Certified Results

Fallback image

AMS Trex users will enjoy all their favorite apps like Field Communicator, Radar Master, Loop Diagnostics, ValveLink Mobile, Fieldbus Diagnostics and WirelessHART™ Provisioning, and others. Additionally, new incorporation of Bluetooth®  technology will add functionality and connectivity and an even more comprehensive toolbox of future apps and accessories. High resolution image

Fallback image

The upgraded AMS Trex retains the same compact and rugged form factor with a new and improved Device Communication Plus Module. High resolution image

AMS Trex Device Communicator redesigned for faster, more precise communication to more devices, now with certified calibration, stronger security

AUSTIN, Texas (Oct. 28, 2025) – Emerson, an industrial technology leader delivering advanced automation solutions, has redesigned its AMS Trex Device Communicator for easier, expanded and more intuitive use by field personnel. New hardware and software and increased security will make the newest version of the AMS Trex Device Communicator safer and more intuitive to use. Additional certifications and expanded connectivity will provide users with the capability to use the AMS Trex communicator for calibration activities, streamlining workflows and reducing the number of tools technicians need to learn and carry into the field.   

The AMS Trex Device Communicator can connect to more than 2,500 field instruments from both Emerson and third-party manufacturers. As a result, many users wish to employ the AMS Trex communicator for calibration because they are familiar with the interface. However, legacy AMS Trex measurement tolerances were designed for reference rather than calibration, making them unsuitable for official calibration activities. As a result, technicians performing calibration typically needed to carry additional devices into the field, increasing complexity and requiring them to learn, manage and maintain multiple technologies. 

The redesigned AMS Trex Device Communicator supports National Institute of Standards and Technology (NIST) traceability. Any measurements taken by the redesigned AMS Trex are NIST certified to ensure that measurement and sourcing of current are accurate enough for calibration activities. 

“As more organizations embrace Emerson’s Boundless Automation vision for an architecture that seamlessly integrates the field, edge, and cloud, their maintenance and reliability teams will be able to manage more assets than ever before, driving a need for improved efficiency,” said Erik Lindhjem, vice president of Emerson’s reliability solutions business. “The new AMS Trex communicator can manage, configure and support field calibrations with a wide array of Emerson and third-party devices, helping teams make the most of their time and data.”

The redesigned AMS Trex Device Communicator also adds HART communication via Bluetooth®, which enables an extended application library and connectivity to Bluetooth devices in the field, expanding its use cases for maintenance and reliability activities. New security features on the platform also eliminate the risk that the device or the plant will be compromised by unauthorized software. The new AMS Trex Communicator features eight times the memory of its predecessor, as well as a quad-core processor and a new operating system that will look and function similarly to modern mobile devices. 

Media:

Additional resources:


About Emerson
Emerson (NYSE: EMR) is a global technology and software company providing innovative solutions for the world’s essential industries. Through its leading automation portfolio, including its majority stake in AspenTech, Emerson helps hybrid, process and discrete manufacturers optimize operations, protect personnel, reduce emissions and achieve their sustainability goals. For more information, visit Emerson.com.