Optimize Separation Efficiency

Chemical Distillation

Chemical distillation processes are pivotal in the refining and chemical industries, demanding precise control to ensure product purity and operational efficiency. Advanced automation and measurement solutions enable consistent performance, energy savings, and adaptability to feedstock variations.

Fallback image
Integrated Control and Measurement

Enhancing Distillation Performance

Achieve consistent product quality and energy efficiency

Variations in feed composition, temperature, and pressure can disrupt distillation operations, leading to off-spec products and increased energy consumption. Implementing advanced sensors, transmitters, and control technologies provides predictive diagnostics and optimized process control, ensuring stable operations and reduced energy usage.

Real-World Applications of Distillation Solutions

Chemical Distillation Solutions in Action

Leading facilities have adopted state-of-the-art control systems and measurement instruments to enhance distillation processes. These implementations have resulted in improved product consistency, reduced energy costs, and minimized downtime, showcasing the tangible benefits of integrating advanced solutions.

Maintain Optimal Thermal Conditions

image

Measuring and optimizing temperature at specific tray levels is necessary for effective separation. The ability to control the temperature profile at all levels ensures the greatest product quality at each extraction point. Emerson offers a wide variety of temperature probes and transmitters, suitable for every imaginable mounting option and measurement range.

Optimize Tray Performance

image

Strategic trays where fractions are withdrawn must be monitored to ensure maximum production without flooding or draining the tray dry. Emerson’s guided wave radar solutions provide very precise measurements, even at high temperatures and pressures.

Control Bottom Product Accumulation

image

Many distillation column accidents have resulted from poor level control at the bottom. If operators do not realize the column is filling with liquid, disaster can result. Control of the reflux boiler depends on how much liquid is at the bottom. Emerson offers multiple level measurement technologies, including differential pressure and guided wave radar, that are well-suited to this application. The Rosemount Thermal Range Expander helps DP installations handle high temperatures.

Regulate Feedstock Introduction

image

Fresh feed must enter the column at the correct temperature, but also at the correct feed rate. For this purpose, a mass flow reading is the most desirable, so a Coriolis mass flow meter is an excellent choice as it can handle the temperatures involved, and its wide flow turn-down range is helpful when moving through startups and correcting upsets.

Optimize Energy Usage

image

Keeping a distillation column running correctly calls for balancing energy input with the production level. Maintaining an optimized energy and mass balance is necessary to drive maximum throughput without wasting steam and fuel. This calls for monitoring of multiple critical measuring points around the tower and ancillary equipment so the automation system can create viable operating scenarios.

Collaborative Expertise

Business Groups in Chemical Distillation

Our diverse business groups offer specialized technologies and services that, when integrated, provide comprehensive solutions for chemical distillation processes.

Explore Our Resources

Solution-Related Documents for Chemical Distillation

Access a collection of high-value documentation developed to help optimize chemical distillation processes. These resources offer strategic insights and technical guidance to support process stability, energy efficiency, and regulatory compliance. With Emerson’s deep industry expertise, you can drive continuous improvement, reduce variability, and ensure safe, consistent distillation performance across your operations.

Improve Process Understanding

Frequently Asked Questions (FAQs)

Gain insights into the fundamentals and complexities of chemical distillation, including column control, energy efficiency, and safety considerations. These frequently asked questions highlight how Emerson technologies help enhance separation performance, reduce operational costs, and maintain product quality.

Distillation columns are inherently difficult to control since there are so many variables, from feedstock inconsistency to the local weather conditions. Emerson has developed many effective control strategies, each capable of balancing a very wide range of variables, but these must all be measured. Effective control across all such variables calls for a variety of instruments, and these investments result in increased production and product quality.

Since most distillation columns are pressurized, using DP to measure the bottom level calls for one of the measurement points to be at the top of the tower. Using a conventional approach, this calls for one impulse line to be as long as the tower is high, a daunting prospect in most cases. Emerson has multiple options to simplify this approach, but the best is an electronic remote sensor that uses a second pressure transmitter at the top. This replaces the long impulse line with an electric cable sending the tower pressure value digitally, simplifying maintenance and increasing reliability.

There are two excellent ways to reduce the amount of wiring infrastructure for temperature sensors. First, Emerson offers a temperature transmitter designed to support four sensors. It sends the four signals sequentially over one pair of wires. This is practical because temperature readings do not change significantly from one second to the next. Second, the same four-sensor transmitter is available using WirelessHART, so no wires are needed at all. Most facilities have WirelessHART networks installed, so adding measurement points in this manner is the lowest cost approach.

Effective tower operation is a balancing act of upward vapor and downward liquid movement. Tray flooding is often a result of vapor gaining the upper hand and choking off liquid flow. This impedes effective separation and hurts product quality. Often such an imbalance may not be recognized if liquid level in strategic trays is not measured. Adding level readings, either using Emerson’s DP transmitters or guided-wave radar level instruments, indicates when such an imbalance has taken hold so the automation system can modulate the feed rate more precisely.