Enhance Safety, Reliability, and Operational Efficiency with Continuous Corrosion and Erosion Monitoring
Corrosion and erosion-related failures are often responsible for significant downtime in process facilities, dramatically impacting both operational reliability and profitability. In critical systems, this degradation both reduces asset lifetime and compromises mechanical integrity, often leading to production losses and potential safety incidents. More traditional reactive maintenance processes mean damage is detected after substantial metal loss has occurred, resulting in limited and expensive mitigation.
Emerson’s corrosion and erosion monitoring solutions can help you gain a complete understanding of your corrosion and erosion risks and the effect of those risks on your plant. This data can be used to make better informed decisions - maximizing plant performance, safety, and profitability.
Produits
Ultrasonic Thickness (UT) Monitoring
Rosemount™ Wireless Corrosion and Erosion Transmitters
Continuously monitor the health of your assets and the impact of corrosion and erosion with Rosemount Wireless Ultrasonic Thickness Transmitters. These non-intrusive, permanently installed devices monitor the wall thickness of your assets and provides you with reliable, accurate data to make more informed decisions and keep your operations running at their peak potential.
Sand Detection and Monitoring
Rosemount SAM42 Acoustic Particle Monitor
Understand your erosion risk with the Rosemount SAM42 Acoustic Particle Monitor. This non-intrusive, permanently installed device listens to the solids in the process stream and measures the intensity of the solids in real-time to help you detect erosion risk before damage, helping to extend the life of your assets.
Inline Fluid Corrosivity Monitoring
Detect real-time corrosion and erosion changes within the process fluid with the Rosemount 4390 Series of Corrosion and Erosion Wireless Transmitters. These transmitters provide accurate and highly sensitive corrosion and erosion monitoring data via probes that directly contact the process fluid, helping you control your corrosion or erosion risk and optimize your operations.
Corrosion Management Software
Plantweb Insight Corrosion and Erosion Applications
Gain better visibility into the health of your assets with a network of predictive intelligence. Emerson’s Plantweb Insight Corrosion and Erosion Applications provide real-time analysis and insights, helping you prevent corrosion or erosion issues before they occur and enable predictive maintenance for more optimized operations.
Frequently Asked Questions
Corrosion occurs through chemical or electrochemical reactions between a material and its environment, resulting in the formation of oxides or other compounds. Erosion is purely mechanical, meaning that material is removed through physical impact by particles, liquids, or gases hitting the surface.
Corrosion and erosion can be measured using weight loss measurements, ultrasonic thickness testing, or electrical probes (which monitor resistance change in an element). Erosion measurements typically involve surface mapping with specialized tools such as radiographs or metal loss testing. Both require monitoring at regular intervals to establish trends and predict when to perform maintenance.
Continuous monitoring can also be deployed using either electrical resistance probes, linear polarization resistance probes, or online ultrasonic thickness sensors, which transmit the wall thickness non-intrusively in real-time.
Corrosion monitoring is the practice of measuring and tracking degradation of metals due to chemical or electrochemical reactions with the environment they are in. Corrosion monitoring helps engineers predict asset lifetime to perform proactive maintenance, optimize corrosion inhibition strategies, and avoid unplanned downtime.
It is effective to combine complementary technologies such as ultrasonic thickness measurements as well as acoustic detection for erosion monitoring. The data can be fed into a centralized monitoring system which uses analytics to identify trends and alert to potential issues early.
While traditional manual testing always requires a couplant gel or fluid in order to transmit an ultrasound between the probe and material, Emerson’s patented ultrasonic technology allows couplant-free permanently installed devices to deliver data directly to the user’s desk. Dry-coupled waveguides and electromagnetic acoustic transducers allow true couplant-free devices to be installed during operation.